How To: File Transfer with USB

Fri, Sep 30, 2011

Control Tips, Expert Tips, How To


USB is standard on all new Haas mills and lathes. LIST PROG features tabbed browsing for file locations. Use the HELP button for the commands. Multiple program selection is possible within the LIST PROG window.

When browsing a list of programs within a device tab, use the up/down arrow keys to highlight programs and press WRITE/ENTER to add the highlighted program to the selection.

Press F4 to save and load data. File transfer is a simple, complete way to back up all data on the control.

External USB hard drives only work when they are formatted as FAT or FAT32. NTFS formatted devices will not work. To find out what your device is formatted as; connect it to your PC, right click on the drive in Windows Explorer and select Properties.

Help Screen:

F4 options:

| More
 
View Related Haas Machines Don't Miss a Word Register for the @Your Service eNewsletter Find Your Local HFO
, , ,